63249-420-409

I/O Terminal Setup

To set up terminal options, follow these steps:

  1. From the MAIN MENU screen, select SETUP > I/O TERMINAL.

    The TERMINAL SETUP screen displays:

  2. Set up the input options listed in the following table.

  3. Exit the TERMINAL SETUP screen to save or change the TRM number.

Terminal Setup Options

Option Value Description
Active YES or NO Determines whether the given terminal is actively used in the controller logic. Valid values are “Y” and “N”. Note that setting to “N” shall retain the configuration of the terminal but simply exclude it from logic and control.
Terminal Digital (all terminals)
Analog - (terminals 1–4 only)
Status Output (terminals 9–16 only)
Indicates the type of physical switch attached to the terminal.
Type See Terminal Types and Descriptions. Indicates the subtype of the physical device attached to the terminal. Relative to the “Type”.

Terminal Settings

Option Description
DIGITAL Momentary Toggle
Momentary On
Momentary Off
Dual Momentary
Maintained NO
Maintained NC
Maintained Toggle
NOTE: See Terminal Types and Descriptions for each option.
ANALOG Voltage 0–5 V
Voltage 0–10 V
Current 4–20 mA

Terminal Types and Descriptions

Option Description
MOMENTARY TOGGLE Momentary Toggle (2-Wire Momentary). Input state alternates between ON and OFF on subsequent contact closures.
MOMENTARY ON Momentary ON. Input state is commanded ON when the contact is closed.
MOMENTARY OFF Momentary OFF. Input state is commanded OFF when the contact is closed.
DUAL MOMENTARY Dual Momentary (3-Wire Momentary). Input state is commanded ON or OFF, according to which contact is closed. This setting requires 2 terminals in the following format: 1 and 9, 2 and 10 ... 8 and 16.
MAINTAIN NO (default) Maintained N.O. (normally open). Input state is commanded ON when the contacts close. Input state is commanded OFF when the contacts open.
MAINTAIN NC Maintained N.C. (normally closed). Input state is commanded ON when the contacts open. Input state is commanded OFF when the contacts close.
MAINTAIN TOGGLE Maintain Toggle. The input state alternates between ON and OFF each time the contact position closes.

Naming a Terminal

To assign or change I/O Terminal names, follow these steps:

  1. From the MAIN MENU, select SETUP > I/O TERMINAL > TERMINAL NAME as shown below.

  2. Select the TRM (terminal) number (001 is displayed).

  3. Enter the name of the terminal (see Entering or Changing a Name ).

  4. To save, exit the TERMINAL NAME screen and return to the TERMINAL SETUP screen or change the TRM number.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.