DUG_Iconic Connected Twin 10 A Socket_PDL-00

Channel mode

Using mode setting, timer can be set to turn off the device after a set period of time or you can set it as a switch to turn on/off manually.
  1. On the Settings page, tap on respective channel.
  2. Select the mode.
    • Switch: turn on/off the device.
    • Timer: set the timer to turn off the device. Refer using mode timer.
  3. Tap Confirm.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?