DUG_Iconic Connected Twin 10 A Socket_PDL-00

Manual operation

Socket can be operated manually using rocker switch and touch switch.

Rocker switch

Off state

  • No power is available at the socket.

  • The socket cannot be remotely switched using Wiser app.

  • Timer and scheduler has no effect on the socket.

Smart state

  • Power is available at the socket.

  • The socket can be remotely switched using Wiser app.

    NOTE: A socket that is remotely switched off using the Wiser app has no power at all, even if the rocker switch is set to smart mode. To find out if a socket is On, tap the touch switch (see Power indication below).
  • Timer and scheduler operates the socket if configured.

Touch switch

Power indication

  • Tap the touch switch to find out if a socket is on.

  • Arrows displayed in the touch switch indicate that power available at a socket:
    Left arrow LED on: power available at left socket.
    Right arrow LED on: power available at right socket.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?