DUG_Iconic Connected Twin 10 A Socket_PDL-00

Troubleshooting

Error

Possible cause

Solution

The device is not ready to pair after the device is removed from the app.

The device is not reset correctly.

Reset to factory default settings, refer to Resetting the device manually.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?