DUG_Iconic Connected Twin 10 A Socket_PDL-00

LED Indication

Pairing

User Action

LED Indication

Status

Press the touch button 3 times

Left and right LED blinks white.

Zigbee pairing mode is active for 30 seconds.

White LED blinks left and right alternately.

Bluetooth pairing mode is active for 30 seconds.

Resetting

User Action

LED Indication

Status

Press the push-button 3 times and long press once for > 10 s.

White LED blinks faster.

The device is in reset mode. It is reset to the factory settings after 10 seconds.

Changing protocol

User Action

LED Indication

Status

Short press the push-button 3 times and long press once for > 20 s.

White LED blinks rapidly.

Pairing mode changes from zigbee to blietooth or bluetooth tozigbee

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?