DUG_Iconic Connected Twin 10 A Socket_PDL-00

Pairing Zigbee device manually

To pair the device manually:
  1. On Home page, tap +.
  2. Tap and select the required Wiser Hub on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is recommended to add the device with install code.
  4. To pair the device with install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code: you can scan the device for the install code.
    • Enter Install Code Manually: you can manually enter the install code from the device.
    After scanning or entering the install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Short press the LED panel 3 times (< 0,5 s).

    The LED blinks white.
  7. In the app, select Confirm both LEDs are flashing and tap Start Configuration (C).

    Wait for a few minutes for the app to connect with Iconic Socket.
  8. Once the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?