DUG_Iconic Connected Twin 10 A Socket_PDL-00

Resetting the device manually

You can reset the device to factory default manually.

Short press the touch button three times (<0,5 s) and then long press the touch button once (>10 s).

After 10 s, release the touch button when the LED starts blinking white.

The device is in reset mode. It is reset to the factory settings after 10 seconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?