DUG_Iconic Connected Twin 10 A Socket_PDL-00

Technical Data

Nominal voltage

AC 240 V ~, 50 Hz

Max load rating

10 A

LED indicator

Yes

Supported protocols

Zigbee, BLE

Compliance

Safety: AS/NZS 3112,AS/NZS 60669.2.1

EMC: AS/NZS 60669.2.1

RF: AS/NZS 4268

Power failure data retention

Internal date/time retained for at least 6 hrs. Settings preserved indefinitely.

Environmental rating

IP20 (designed for indoor use only)

Operating humidity

5%–90% RH, non-condensing

Specifications typical at 25 °C

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?