DOCA0176EN-09

Firmware Version 001.001.054

Performance Improvement

The secondary current injection accuracy is improved for the automatic trip curve test on the MicroLogic trip units installed in the following circuit breakers:

  • ComPacT NS circuit breaker

  • PowerPacT P- and R-frame circuit breaker

  • MasterPacT NT/NW circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.