DOCA0111EN-03

Combining the TeSys H Motor Starter with Circuit Breakers

Overview

WARNING
HAZARDOUS VOLTAGE AT THE MOTOR
  • Check the safety function each time the TeSys H motor starter trips.
  • Replace the TeSys H motor starter after every short circuit in the case of short-circuit protection according to type-1 coordination, and before restarting the motor.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

For use in North America

WARNING
HAZARD OF FIRE OR ELECTRIC SHOCK
  • The opening of the branch-circuit protective device may be an indication that a fault current has been interrupted.
  • To reduce the hazard of fire or electric shock, current-carrying parts and the other components of the controller should be examined and replaced if damaged.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The TeSys H motor starter can be combined with the following magnetic motor circuit breakers:

  • GV2L: rotary knob type Ue = 500 V

  • GV2LE: rocker lever type Ue = 415 V

Type-1 Coordination According to IEC/EN 60947-4-2 for 415 V Maximum Voltage

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

LZ••2X4••

50

GV2L/GV2LE04

0.63

LZ••2X4••

50

GV2L/GV2LE05

1

LZ••2X4••

50

GV2L/GV2LE06

1.6

LZ••2X4••

20

GV2L/GV2LE07

2.5

Data is valid at 40 °C

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

LZ••6X5••

50

GV2L/GV2LE06

1.6

LZ••6X5••

20

GV2L/GV2LE07

2.5

LZ••6X5••

10

GV2L/GV2LE08

4

LZ••6X5••

7

GV2L/GV2LE10

6.3

LZ••6X5••

7

GV2L/GV2LE14

10

Data is valid at 40 °C

Type-1 Coordination According to IEC/EN 60947-4-2 for 500 V Maximum Voltage

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

LZ••2X4••

35

GV2L/GV2LE04

0.63

LZ••2X4••

35

GV2L/GV2LE05

1

LZ••2X4••

35

GV2L/GV2LE06

1.6

LZ••2X4••

10

GV2L/GV2LE07

2.5

Data is valid at 40 °C

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

LZ••6X5••

35

GV2L/GV2LE06

1.6

LZ••6X5••

10

GV2L/GV2LE07

2.5

LZ••6X5••

8

GV2L/GV2LE08

4

LZ••6X5••

4

GV2L/GV2LE10

6.3

LZ••6X5••

3

GV2L/GV2LE14

10

Data is valid at 40 °C

Group Protection with Type-1 Coordination According to IEC/EN 60947-4-2 for 415 V Maximum Voltage

This table gives the maximum short circuit current that can be protected by association of a GV2 circuit breaker and several TeSys H motor starters. The total nominal current of all TeSys H motor starters combined together should not exceed the maximum current of the GV2L/GV2LE circuit breaker associated for group short circuit protection.

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

2.4 A

6.5 A

LZ••2X4••

LZ••6X5••

10

GV2L/GV2LE08

4

LZ••2X4••

LZ••6X5••

7

GV2L/GV2LE10

6.3

LZ••2X4••

LZ••6X5••

7

GV2L/GV2LE14

10

LZ••6X5••

5

GV2L/GV2LE16

14

LZ••6X5••

4

GV2L/GV2LE20

18

LZ••6X5••

4

GV2L/GV2LE22

25

Group Protection with Type-1 Coordination According to IEC/EN 60947-4-2 for 500 V Maximum Voltage

This table gives the maximum short circuit current that can be protected by association of a GV2 circuit breaker and several TeSys H motor starters. The total nominal current of all TeSys H motor starters combined together should not exceed the maximum current of the GV2L / GV2LE circuit breaker associated for group short circuit protection.

TeSys H motor starter

Iq short circuit current (kA)

Circuit breaker reference

Maximum current at 40 °C (A)

2.4 A

6.5 A

LZ••2X4••

LZ•H6X5••

8

GV2L/GV2LE08

4

LZ••2X4••

LZ•H6X5••

4

GV2L/GV2LE10

6.3

LZ••2X4••

LZ•H6X5••

3

GV2L/GV2LE14

10

LZ•H6X5••

2

GV2L/GV2LE16

14

LZ•H6X5••

2

GV2L/GV2LE20

18

LZ•H6X5••

2

GV2L/GV2LE22

25

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.