DOCA0111EN-03

Derating Characteristics

Overview

The curves in this section show the maximum load current for the following parameters:

  • Power supply

  • Ambient temperature

  • Distance between devices

Derating Characteristics for AC53A (Motor Application) Duty by Temperature and Mounting Space for 24 Vdc

1 Distance between devices is 20 mm (0.51 in)

2 No space between devices

Derating Characteristics for AC53A (Motor Application) Duty by Temperature and Mounting Space for 110–230 Vac

1 Distance between devices is 20 mm (0.51 in)

2 No space between devices

Derating Characteristics for High-Efficiency Motors

TeSys H motor starters are designed for motors with a starting current (Is) that is eight times the nominal current (Ie), according to IEC 60947-4-2. For these motors, Is/Ie = 8.

The following tables list the maximum nominal current for motors where Is/Ie is greater than or equal to 8. If necessary, limit the maximum nominal current of these motors.

LX•2X4

Ratio of maximum starting current to nominal current (Is/le)

8

8.5

9

9.5

10

Nominal current (Ie) in A

2.4

2.4

2.4

2.4

2.4

LX•6X5

Ratio of maximum starting current to nominal current (Is/le)

8

8.5

9

9.5

10

Nominal current (Ie) in A

6.5

6

5.7

5.5

5.2

Derating Characteristics for AC51 (Resistive Load) Duty by Temperature and Mounting Space for 24 Vdc

1 Distance between devices is 20 mm (0.51 in)

2 No space between devices

Derating Characteristics for AC51 (Resistive Load) Duty by Temperature and Mounting Space for 110–230 Vac

1 Distance between devices is 20 mm (0.51 in)

2 No space between devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.