DOCA0111EN-03

Combining the TeSys H Motor Starter with Fuses

Type-1 Coordination According to IEC/EN 60947-4-2

TeSys H motor starter

Iq short circuit current (kA)

Protection type

Maximum current (A)

Maximum voltage (V)

LZ••2X4••

10

Fuse gG

25

500

LZ••6X5••

10

Fuse gG

25

500

Data is valid at 40 °C.

For Use in North America: Type-1 Coordination According to IEC/EN 60947-4-2

@TechPub writer (02/2016): for an updated release after DOCA0111EN-00 (02/2016): Must data on Type-2 coordination be added?? (see Denis Merkel, maybe)

TeSys H motor starter

Iq short circuit current (kA)

Protection type

Maximum current (A)

Maximum voltage (V)

LZ••2X4••

100

Fuse class J or CC

30

500

LZ••6X5••

100

Fuse class J or CC

30

500

LZ••2X4••

5

Fuse RK5

20

500

LZ••6X5••

5

Fuse RK5

20

500

Data is valid at 40 °C.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.