Motor Control Using a Standard or STO Motor Starter for Motors with Brake
Overview
CAUTION |
|---|
|
OVERHEATING
When you connect and operate motors with built-in brakes,
be aware of the hazard of overheating. The energy to release the brakes
is taken from the motor connection cables, which can cause asymmetrical
power consumption and result in overheating.
Failure to follow these instructions can result in injury or equipment damage.
|
CAUTION |
|---|
|
UNINTENDED EQUIPMENT OPERATION
The current setting of the TeSys H motor starter must be the nominal current of the motor increased by the value
of the brake nominal current.
Failure to follow these instructions can result in injury or equipment damage.
|
| NOTICE |
|---|
|
Hazard of equipment DAMAGE
Connect the TeSys H motor starter as specified in the wiring diagrams.
Failure to follow these instructions can result in equipment damage.
|
This section provides circuits for motors with a brake. The wiring diagram you use depends on voltage supply of the brake, either 230 Vac or 400 Vac.
Activate external brakes by using a separate contactor, such as TeSys D.
CAUTION