DOCA0111EN-02

Motor Control Using a Standard TeSys H Motor Starter

Overview

NOTICE
DAMAGE TO MOTOR
Connect the TeSys H motor starter as specified in the wiring diagrams.
Failure to follow these instructions can result in equipment damage.

This section provides an example circuit for a DOL motor, using an LZ1H or LZ2H, non-STO, TeSys H motor starter.

Three-Phase Motor Without Brake

This example wiring diagram is for a 3-phase motor without a brake.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?