DOCA0093EN-06

ULP Accessories

ULP Accessories

ULP accessories can be grouped in categories:

RJ45 Plug/Plug ULP Cord

Use simple plug-and-play ULP cords to interconnect ULP modules within a single IMU. They have RJ45 plug connectors at both ends and are available in several lengths.

Illustration

Description

Part number

L = 0.3 m (0.98 ft) (ten cords)

TRV00803

L = 0.6 m (1.98 ft) (ten cords)

TRV00806

L = 1 m (3.28 ft) (five cords)

TRV00810

L = 2 m (6.56 ft) (five cords)

TRV00820

L = 3 m (9.84 ft) (five cords)

TRV00830

L = 5 m (16.4 ft) (one cord)

TRV00850

ULP Line Termination

NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Never connect a ULP line termination to an Ethernet or Modbus-SL RJ45 port.
  • The ULP line termination must be connected on an RJ45 ULP port only.
Failure to follow these instructions can result in equipment damage.

The ULP line termination closes the unused RJ45 ULP port on a ULP module. It consists of an RJ45 connector with passive components in a sealed unit.

Illustration

Description

Part number

Ten ULP line terminations

TRV00880

ULP Line Termination in an IMU with MasterPacT MTZ Circuit Breaker

The following table lists the ULP module on which the ULP line termination must be connected in the case of an IMU with a MasterPacT MTZ circuit breaker with MicroLogic X control unit and a ULP port module.

IMU

Connection of the ULP line termination

MasterPacT MTZ circuit breaker with ULP port module

No ULP line termination

(connect a protection cap on the unused connector on the ULP port module)

MasterPacT MTZ circuit breaker with ULP port module connected to an EIFE interface

On ULP port module

MasterPacT MTZ circuit breaker with ULP port module connected to an EIFE interface and one IO module

On IO module

MasterPacT MTZ circuit breaker with ULP port module connected to one IO module and an IFE interface

On IFE interface

RJ45 Socket Connector

Use the RJ45 socket connector to connect two ULP cords end-to-end and thus extend them. It consists of two RJ45 socket connectors linked by a direct electrical connection.

Illustration

Description

Part number

Ten RJ45 socket connectors

TRV00870

The length of the extended ULP cord is limited.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.