DOCA0093EN-06

Hardware and Firmware Compatibility of ULP Modules

Introduction

ULP modules must be compatible with both the hardware and firmware.

The hardware and firmware compatibility of ULP modules can be checked with:

Hardware Compatibility

The following table lists the compatible ULP modules for each range of circuit breakers:

  • MasterPacT MTZ circuit breaker with ULP port module and MicroLogic X control unit

  • MasterPacT NT/NW, ComPacT NS, or PowerPacT P- and R-frame circuit breaker with BCM ULP module and MicroLogic trip unit

  • ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM module or BSCM Modbus SL/ULP module in ULP only mode and/or with MicroLogic trip unit. It is recommended to use the BSCM Modbus SL/ULP module in ULP only mode only for fixed ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breakers, but not for withdrawable and plug-in circuit breakers.

  • ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM Modbus SL/ULP module in Modbus SL only mode or Modbus SL and ULP mode and/or with MicroLogic trip unit

ULP module

Part number

Circuit breakers

MasterPacT MTZ

MasterPacT NT/NW, ComPacT NS, or PowerPacT P- and R-frame

ComPacT NSX or PowerPacT H-, J-, and L-frame (ULP only mode)

ComPacT NSX or PowerPacT H-, J-, and L-frame (Modbus SL only mode or Modbus SL and ULP mode)

IFE Ethernet interface for one circuit breaker

LV434001

IFE Ethernet switchboard server

LV434002

EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

LV851001

Spare part kit EIFE for one MasterPacT MTZ1 drawout circuit breaker

LV851100SP

Spare part kit EIFE for one MasterPacT MTZ2/MTZ3 drawout circuit breaker

LV851200SP

IFM Modbus-SL interface for one circuit breaker with Modbus-SL RJ45 port

LV434000

IFM Modbus-SL interface for one circuit breaker with Modbus-SL 5-pin connector

TRV00210 or STRV00210

FDM121 front display module for one circuit breaker

TRV00121 or STRV00121

IO input/output application module for one circuit breaker

LV434063

Service Interface

LV485500

USB maintenance interface

TRV00911 or STRV00911

Firmware Compatibility Matrix

The primary reason for updating the system is to obtain the latest system features. The latest device firmware baseline and version details of the devices are available in EcoStruxure Power Commission software.

Checking Hardware and Firmware Compatibility with ULP Status LED

The yellow ULP LED indicates the mode of the ULP module.

ULP LED

Mode

Action

Nominal

None

Conflict

Remove extra ULP module

Degraded

Replace ULP module at the next maintenance operation

Test

None

Non-critical firmware discrepancy

Update firmware at the next maintenance operation

Non-critical hardware discrepancy

Replace ULP module at the next maintenance operation

Configuration discrepancy

Install missing features

Critical firmware discrepancy

Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions

Critical hardware discrepancy

Stop

Replace ULP module

Power off

Check power supply

Checking Hardware and Firmware Compatibility with EcoStruxure Power Commission Software

EcoStruxure Power Commission software can be used to check hardware and firmware compatibility of the modules in the IMU and to get recommended actions to recover from a compatibility discrepancy situation.

For more information, refer to EcoStruxure Power Commission Online Help.

Click here to download the latest version of EcoStruxure Power Commission software.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.