DOCA0093EN-06

ULP System Presentation

Description

Use the ULP (Universal Logic Plug) system to construct an electrical distribution solution which integrates metering, communication, and operating assistance functions for IEC and UL/ANSI circuit breakers and switch-disconnectors.

IEC Devices Compatible with the ULP System

The IEC devices compatible with the ULP system are the following:

  • ComPacT NSX circuit breakers and switch-disconnectors from 100 to 630 A

  • ComPacT NSX DC

    circuit breakers from 100 to 1200 A and switch-disconnectors from 100 to 630 A
  • ComPacT NS circuit breakers and switch-disconnectors from 630 to 3200 A

  • MasterPacT NT circuit breakers and switch-disconnectors from 630 to 1600 A

  • MasterPacT NW circuit breakers and switch-disconnectors from 800 to 6300 A

  • MasterPacT MTZ1 circuit beakers from 630 to 1600 A

  • MasterPacT MTZ2 circuit beakers from 800 to 4000 A

  • MasterPacT MTZ3 circuit beakers from 4000 to 6300 A

NOTE:

The information related to the new generation of ComPacT NSX circuit breakers in this guide applies also to the existing ranges of ComPact NSX circuit breakers.

The information related to the new generation of ComPacT NS circuit breakers in this guide applies also to the existing ranges of ComPacT NS circuit breakers.

The exceptions are mentioned wherever applicable. The new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.

UL/ANSI Devices Compatible with the ULP System

The UL/ANSI devices compatible with the ULP system are the following:

  • PowerPacT H-frame circuit breakers and switches from 15 to 150 A

  • PowerPacT J-frame circuit breakers and switches from 150 to 250 A

  • PowerPacT L-frame circuit breakers and switches from 250 to 600 A

  • PowerPacT P-frame circuit breakers and switches from 600 to 1200 A

  • PowerPacT R-frame circuit breakers and switches from 1600 to 3000 A

  • MasterPacT NT circuit breakers and switches from 600 to 1600 A

  • MasterPacT NW circuit breakers and switches from 800 to 6000 A

  • MasterPacT MTZ1 circuit breakers from 600 to 1600 A

  • MasterPacT MTZ2 circuit breakers from 800 to 4000 A

  • MasterPacT MTZ3 circuit breakers from 4000 to 6000 A

NOTE:

The information related to the new generation of PowerPacT circuit breakers in this guide applies also to the existing ranges of PowerPact circuit breakers.

The exceptions are mentioned wherever applicable. The new ranges are based on the same technical and dimensional architecture as that of the exiting range of circuit breakers.

Architecture Example

Legend

Description

Part of the ULP system

A

FDM128 Ethernet display for eight devices

B

FDM121 front display module for one circuit breaker

C

IFE Ethernet interface for one circuit breaker

D

IFE Ethernet switchboard server

E

IFM Modbus-SL interface for one circuit breaker

F

Modbus SL hub

G

IO input/output application module for one circuit breaker

H

MasterPacT MTZ drawout circuit breaker

I

MasterPacT MTZ fixed circuit breaker

J

MasterPacT NT/NW circuit breaker

K

ComPacT NS/PowerPacT P- and R-frame circuit breaker

L

ComPacT NSX/PowerPacT H-, J-, and L-frame plug-in circuit breaker

M

ComPacT NSX/PowerPacT H-, J-, and L-frame withdrawable circuit breaker

N

ComPacT NSX/PowerPacT H-, J-, and L-frame fixed circuit breaker

O

BSCM Modbus SL/ULP module

P

ULP port module

Q

EIFE Embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

R

ULP line termination

S

BSCM Modbus SL cord

T

RJ45 ULP cord

U

Circuit breaker BCM ULP cord

V

NSX cord

Cable

Description

Ethernet network

Modbus network

ULP network

24 Vdc power supply

Features

Use the ULP system to enhance the functions of ComPacT NSX, PowerPacT H-, J-, and L-frame, ComPacT NS, PowerPacT P- and R-frame, MasterPacT NT/NW, and MasterPacT MTZ circuit breakers by:

  • An Ethernet communication link for access and remote monitoring with the IFE communication interface or EIFE interface (MasterPacT MTZ drawout circuit breakers only).

  • Web access to monitor and control the circuit breaker connected to an IFE communication interface or EIFE interface (MasterPacT MTZ circuit breakers only).

  • An input/output application with an IO module. It benefits from the extended capability of the IO module to monitor and control position of drawout circuit breakers in the cradle, circuit breaker operation, and custom application, and so on.

  • Test, setup, and maintenance functions with EcoStruxure Power Commission software.

  • A Modbus-SL communication link for access and remote monitoring:

    • With the IFM communication interface.

    • With the BSCM Modbus SL/ULP module and the Modbus SL hub (for ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers only).

  • Local display of measurements and operating assistance data with the FDM121 display.

The ULP system lets the circuit breakers become a metering and supervision tool to assist energy efficiency and can:

  • Optimize energy consumption by zone or by application, according to the load peaks or priority zones.

  • Improve electrical equipment management.

Intelligent Modular Unit (IMU)

A modular unit is a mechanical and electrical assembly containing one or more products to perform a function in electrical equipment (incoming protection, motor command and control). The modular units are easily installed in the electrical equipment.

The circuit breaker with its internal communicating components (for example, MicroLogic™ trip unit) and external ULP modules (for example, IO module) connected to one communication interface (IFE, EIFE, IFM, or BSCM Modbus SL/ULP module depending on the circuit breaker type) is called an intelligent modular unit or IMU.

Examples of IMU with ComPacT NSX or PowerPacT H-, J-, and L-Frame Circuit Breaker

Example 1: IMU composed of a fixed ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker connected to a BSCM Modbus SL/ULP module, an FDM121 display and an IO module.

A

Modbus SL hub

B

BSCM Modbus SL cord

C

BSCM Modbus SL/ULP module

D

MicroLogic 5, 6 or 7 trip unit

E

NSX cord

F

IO module

G

ULP cord

H

FDM121 display

Example 2: IMU composed of a ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker connected to one IO module and an IFE communication interface.

A

Modbus TCP client

B

Ethernet cable

C

IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard server

D

BSCM Modbus SL/ULP module

E

MicroLogic 5, 6 or 7 trip unit

F

NSX cord

G

ULP cord

H

IO module

I

FDM121 display

Example 3: IMU composed of a withdrawable ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with a BSCM Modbus SL/ULP module connected to an FDM121 display and an IFM communication interface.

NOTE: It is recommended to use the BSCM Modbus SL/ULP module in ULP only mode for withdrawable and plug-in circuit breakers.

A

FDM121 display

B

9-wire fixed connector for base

C

9-wire moving connector

D

Support for two moving connectors

E

CE/CD (connected/disconnected) position auxiliary switches

F

NSX cord

G

RJ45 plug/plug ULP cord

H

ULP line termination

I

IFM communication interface

Examples of IMU with MasterPacT NT/NW Circuit Breaker

Example 1: IMU composed of a fixed, electrically-operated MasterPacT NT circuit breaker connected to an IFM communication interface and an FDM121 display.

A

IFM Modbus-SL interface for one circuit breaker

B

Circuit breaker BCM ULP cord

C

Fixed terminal block

D

BCM ULP circuit breaker communication module

E

Fixed electrically-operated circuit breaker

F

RJ45 plug/plug ULP cord

G

ULP line termination

H

FDM121 front display module for one circuit breaker

Example 2: IMU composed of a drawout MasterPacT NT circuit breaker connected to one IO module for cradle management and an IFE communication interface.

A

IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard serve

B

ULP line termination

C

RJ45 plug/plug ULP cord

D

Circuit breaker BCM ULP cord

E

Circuit breaker disconnected position contact (CD)

F

Circuit breaker cradle

G

BCM ULP circuit breaker communication module

H

Drawout circuit breaker

I

Drawout terminal block

J

Circuit breaker connected position contact (CE)

K

Circuit breaker test position contact (CT)

L

IO input/output application module for one circuit breaker

Examples of IMU with MasterPacT MTZ Circuit Breaker

Example 1: IMU composed of a MasterPacT MTZ fixed circuit breaker connected to one IO module and an IFE communication interface.

A

IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard server

B

ULP line termination

C

IO input/output application module for one circuit breaker

D

RJ45 plug/plug ULP cord

E

ULP port module

F

MasterPacT MTZ fixed circuit breaker

Example 2: IMU composed of a MasterPacT MTZ drawout circuit breaker connected to an EIFE interface and one IO module.

A

IO input/output application module for one circuit breaker

B

ULP line termination

C

ULP port module

D

RJ45 plug/plug ULP cord

E

MasterPacT MTZ drawout circuit breaker

F

Cord between ULP port module and EIFE interface

G

EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.