DOCA0093EN-06

Composition Rules for Intelligent Modular Units (IMUs)

Introduction

Connection of an IMU in the ULP system is simple, but must comply with the rules concerning composition, RJ45 plug/plug ULP cords, and the ULP module power supply.

General Rule: Composition of an IMU

An IMU is composed of the following two device types:

  • One main device (circuit breaker or switch-disconnector) and an internal ULP communication module

  • One or several external ULP modules

Device range Main device type ULP modules

ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers

In ULP only mode:

  • ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM Modbus SL/ULP module and/or MicroLogic 5, 6, or 7 trip unit

  • ComPacT NSX or PowerPacT H-, J-, and L-frame switch-disconnector with BSCM Modbus SL/ULP module

  • ComPacT NSX DC circuit breaker or switch-disconnector with BSCM Modbus SL/ULP module

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

  • 0 or 1 interface among:

    • IFE interface

    • IFE server (1)

    • IFM interface

In Modbus SL and ULP mode:

  • Fixed ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM Modbus SL/ULP module

  • Fixed ComPacT NSX or PowerPacT H-, J-, and L-frame switch-disconnector with BSCM Modbus SL/ULP module

  • Fixed ComPacT NSX DC circuit breaker or switch-disconnector with BSCM Modbus SL/ULP module

  • 1 Modbus SL hub

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

In Modbus SL only mode:

  • Fixed ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker or switch-disconnector with BSCM Modbus SL/ULP module

  • Fixed ComPacT NSX DC circuit breaker or switch-disconnector with BSCM Modbus SL/ULP module

1 Modbus SL hub

ComPacT NS and PowerPacT P- and R-frame circuit breakers

ComPacT NS or PowerPacT P- and R-frame circuit breaker with BCM ULP circuit breaker communication module

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

  • 0 or 1 interface among:

    • IFE interface

    • IFE server (1)

    • IFM interface

MasterPacT NT/NW circuit breakers

MasterPacT NT/NW circuit breaker with BCM ULP circuit breaker communication module

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

  • 0 or 1 interface among:

    • IFE interface

    • IFE server (1)

    • IFM interface

MasterPacT MTZ circuit breakers with MicroLogic X control units

MasterPacT MTZ drawout circuit breaker with ULP port module

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

  • 0 or 1 interface among:

    • IFE interface

    • IFE server (1)

    • EIFE embedded Ethernet interface

    • IFM interface (LV434000 only)

 

MasterPacT MTZ fixed circuit breaker with ULP port module

  • 0 or 1 FDM121 display

  • 0, 1, or 2 IO modules

  • 0 or 1 interface among:

    • IFE interface

    • IFE server (1)

    • IFM interface (LV434000 only)

(1) One IFE server with stacked IFM interfaces:

  • In terms of power supply, the maximum number of IFM interfaces stacked to one IFE server is 11 in order to limit voltage drop.

  • In terms of Modbus-SL communication, it depends on the performance requirement. As it takes approximately 500 ms at 19,200 Baud per device to refresh 100 registers, the more interfaces added the longer the minimum refreshment period. The minimum refreshment period depends on the number of IFM interfaces stacked to one IFE server. Multiply the time to refresh one device by the number of devices to find the minimum refreshment period expected in the application. For instance, an installation with eight IFM interfaces stacked to one IFE server at 19,200 Baud would take approximately 4 seconds to be read.

    For good communication performance, a maximum of eight IFM interfaces stacked to one IFE server is recommended.

These examples illustrate the composition rules for an IMU.

A

ComPacT NSX, PowerPacT H-, J-, and L-frame, ComPacT NS, PowerPacT P- and R-frame, or MasterPacT NT/NW circuit breaker

B

MasterPacT MTZ circuit breaker with ULP port module

C

MasterPacT MTZ drawout circuit breaker with ULP port module and EIFE interface

These examples illustrate the composition rules for an IMU for ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker only.

A

ComPacT NSX or PowerPacT H-, J-, and L-frame circuit breaker with BSCM Modbus SL/ULP module

General Rule: Order of ULP Modules in an IMU

Connect the ULP modules in a single IMU in any order. Base the connection on the ULP cable recommendations and the desired layout for the ULP modules in the electrical equipment.

A

ComPacT NSX, PowerPacT H-, J-, and L-frame, ComPacT NS, PowerPacT P- and R-frame, MasterPacT NT/NW, or MasterPacT MTZ circuit breaker

General Rule: ULP Line Termination

The ULP modules placed at the end of the ULP line must have a ULP line termination (part number TRV00880) on the unused ULP RJ45 connector.

Example of ULP line termination on IFE interface:

Place the ULP modules which have an internal ULP line termination at the end of the ULP line. The ULP modules which have an internal ULP line termination are:

  • BSCM Modbus SL/ULP module for ComPacT NSX, PowerPacT H-, J-, and L-frame, and ComPacT NSX DC circuit breakers.

  • MicroLogic 5, 6, or 7 trip unit for ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers.

  • BCM ULP module for ComPacT NS, PowerPacT P- and R-frame, or MasterPacT NT/NW circuit breakers.

  • ULP port module for MasterPacT MTZ circuit breakers.

NOTE: In an architecture with an EIFE interface connected to a ULP port module, the ULP port module is the end of the ULP line.

General Rule: Cables to Interconnect IMUs on Communication Networks

Do not connect the IMUs to one another with ULP cords.

  • Use only the Ethernet cable to interconnect IMUs connected to an Ethernet network.

    A

    ComPacT NSX, PowerPacT H-, J-, and L-frame, ComPacT NS, PowerPacT P- and R-frame, MasterPacT NT/NW, or MasterPacT MTZ circuit breaker

  • Use only the Modbus cable or stacking accessory to interconnect IMUs connected to a Modbus network.

    A

    ComPacT NSX, PowerPacT H-, J-, and L-frame, ComPacT NS, PowerPacT P- and R-frame, MasterPacT NT/NW, or MasterPacT MTZ circuit breaker

General Rule: Limitation of Number of MasterPacT MTZ, ComPacT NSX and PowerPacT H-, J-, and L-Frame Circuit Breakers

In case of floating power supply and when no IFM interface with part number TRV00210 is installed in the ULP system, the number of MasterPacT MTZ circuit breakers with MicroLogic X control units, and the number of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers is limited by ground leakage currents as described in the following tables.

The limitation is valid for MasterPacT MTZ circuit breakers with MicroLogic X control units, and for ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers used with a ULP connection.

Limiting the maximum number of IMUs on the same external DC power supply limits the cumulated leakage currents under 0.5 mA (human sensitivity level) or 3.5 mA (class I equipment).

Number of MicroLogic trip units or control units in the case of 0.5 mA leakage current maximum:

Ue (V L-N / U L-L) (Vac)

Maximum number of MicroLogic X control units without VPS power supply (MasterPacT MTZ circuit breakers)

Maximum number of MicroLogic X control units with VPS power supply (MasterPacT MTZ circuit breakers)

Maximum number of MicroLogic trip units (ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers)

66 / 115

144

23

66

127 / 220

75

12

34

230 / 400

41

6

19

347 / 600

27

4

12

400 / 690

24

9

11

1,000

16

6

0

Number of MicroLogic trip units or control units in the case of 3.5 mA leakage current maximum:

Ue (V L-N / U L-L) (Vac)

Maximum number of MicroLogic X control units without VPS power supply (MasterPacT MTZ circuit breakers)

Maximum number of MicroLogic X control units with VPS power supply (MasterPacT MTZ circuit breakers)

Maximum number of MicroLogic trip units (ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers)

66 / 115

344

57

156

127 / 220

180

29

81

230 / 400

99

16

44

347 / 600

66

10

29

400 / 690

57

23

26

1,000

39

16

0

General Rule: Power Supply Through the ULP Cord

Only one device can be powered through the ULP cord. This device must be at the end of the ULP line. It can be done only for the following devices:

  • FDM121 display.

  • BSCM Modbus SL/ULP module in ULP only mode for ComPacT NSX, PowerPacT H-, J-, and L-frame, and ComPacT NSX DC circuit breakers.

  • MicroLogic 5, 6, or 7 trip unit for ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers.

  • BCM ULP module for MasterPacT NT/NW, ComPacT NS, and PowerPacT P- and R-frame circuit breakers.

NOTE: If BSCM Modbus SL/ULP module is in Modbus SL and ULP mode, the power supply to the BSCM Modbus SL/ULP module and the ULP modules connected to it is provided by the Modbus SL hub.

Example: In the diagram, the FDM121 display and the ComPacT NSX MicroLogic trip unit are powered through ULP system. The IFE server and the IO modules are connected to the power supply. As the IFM interfaces are stacked on the IFE server, they are already powered.

A

IFE server

B

IFM interfaces stacked on IFE server

C

FDM121 display

D

IO module

E

MicroLogic trip unit in ComPacT NSX circuit breaker

NOTE: The ULP port module on MasterPacT MTZ circuit breaker must be connected to a 24 Vdc power supply.

Length of ULP Cords

The rules for ULP cord length are as follows:

  • The maximum length of the ULP cord between two ULP modules in an IMU is 5 m (16.4 ft) if one of the ULP modules does not have an external power supply.

  • The maximum length of the ULP cord between two ULP modules in an IMU is 10 m (32.8 ft) if both ULP modules have an external power supply.

  • The maximum length of all the ULP cords on a single IMU is 20 m (65.6 ft).

  • In the case of an installation with a withdrawable drawer, the total length of the ULP cords for the fixed part must be less than 12 m (39.4 ft). This length limitation is to ensure that the fixed part operates correctly when the drawer is drawn out.

  • The bending radius of the ULP cords must be 50 mm (1.97 in) minimum.

NOTE: In the following cases of device combinations with an IFE interface with part number LV434010 or LV434011, ULP total network length is limited to a maximum of 5 m (16.4 ft):
  • A MasterPacT MTZ circuit breaker and an IFE interface.

  • A MasterPacT MTZ circuit breaker, one IO module, and an IFE interface.

  • A MasterPacT MTZ circuit breaker, two IO modules, and an IFE interface.

Maximum Number of Stacked Devices

A maximum of 12 circuit breakers can be connected to stacked modules (IFE server, IFM interface, or Modbus SL hub).

Example of a maximum configuration with 12 circuit breakers:

  • 1 IFE server connected to 1 circuit breaker.

  • Stacked to 1 IFM interface connected to 1 circuit breaker.

  • Stacked to 4 Modbus SL hubs, connected to a maximum of 10 circuit breakers. 2 RJ45 ports remain free on the Modbus SL hubs.

Summary of Connection Rules

Characteristic

Value

Connection

Daisy-chaining of ULP cords and ULP line termination at the end of the ULP line.

Maximum length

Voltage range supported

24 Vdc -10%/+10% (21.6–26.4 Vdc)

Current limitation on each ULP RJ45 port

300 mA

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.