DOCA0093EN-06

Communication Architecture Examples with Modbus SL Hub

Modbus SL Hub Stacked with IFE Server and IFM Interface

Modbus SL hub can be directly stacked with IFE server or IFM interface with the help of stacking accessory (TRV00217) as shown in the following architecture. In this architecture, both 24 Vdc supply and Modbus connection flows via the stacking accessory.

  1. IFE server

  2. IFM interface

  3. Modbus SL hub

  4. Drawout MasterPacT MTZ1/MTZ2/MTZ3

  5. Fixed MasterPacT MTZ1/MTZ2/MTZ3

  6. Fixed ComPacT NSX / PowerPacT H-, J-, and L-Frame

  7. BSCM Modbus SL/ULP module

  8. Ethernet cable

  9. BSCM Modbus SL cord

  10. ULP cord

Modbus SL Hub Daisy Chained with IFE Server and IFM Interface

When it is not possible to stack the Modbus SL hubs together with the help of the stacking accessory TRV00217, the Modbus SL hubs can be daisy chained using the terminal block connector, as shown in the following architecture. In this architecture, the IFE server acts as a gateway.

  1. IFE server

  2. IFM interface

  3. Modbus SL hub

  4. Drawout MasterPacT MTZ1/MTZ2/MTZ3

  5. Fixed MasterPacT MTZ1/MTZ2/MTZ3

  6. Fixed ComPacT NSX / PowerPacT H-, J-, and L-frame

  7. BSCM Modbus SL/ULP module

  8. Ethernet cable

  9. BSCM Modbus SL cord

  10. Modbus cord and 24 Vdc power supply

  11. Modbus SL cable

  12. ULP cord

Stacked Modbus SL Hub and IFM Interface, Connected to Panel Server

Modbus SL hub can be connected to the Panel Server via the terminal block connector of the Modbus SL hub as shown in the following architecture. In this architecture, only the Modbus communication network uses the terminal block connector.

  1. Panel Server

  2. IFM interface

  3. Modbus SL hub

  4. Drawout MasterPacT MTZ1/MTZ2/MTZ3

  5. ComPacT NSX / PowerPacT H-, J-, and L-Frame

  6. BSCM Modbus SL/ULP module

  7. Ethernet cable

  8. BSCM Modbus SL cord

  9. Modbus cord

  10. ULP cord

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.