DUG_Exxact FLS_WSE-01

Adding a lighting group

To add a lighting group to the top and bottom left key:
  1. On the Home page, tap All devices > Connected Wireless Switch.
  2. On the control panel page, tap Top left key > Lighting Group > +.
  3. Tap Edit name , enter the group name (A) and tap Save.
    TIP: You can choose the cover image that represents your group by tapping .

  4. Tap Add Task to select any device from the list and tap Next.
    NOTE: You can add one or more actions using .

  5. Once all the actions are set, tap Save.
  6. On the Lighting Group page, select the light group (B) you want to assign to the push button.
  7. Short press the top right push button 3 times to activate the device and tap Sure (C) on the app.

    The lighting group is now added to the top and bottom left key (D).

    NOTE: If you add a shutter/moment group to the top/bottom left key, then the app removes the lighting group from the top/bottom left key.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?