DUG_Exxact FLS_WSE-01

Pairing device manually

To pair the device manually:
NOTE: Remember to insert the battery to turn on the device.
  1. On the Home page, tap +.
  2. Tap , select Wiser Hub on the slide-up menu and tap Done.
  3. Select any one of the options to add device (A):
    • Add Device with Install Code
    • Add Device without Install Code

  4. To pair the device with an Install Code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - You can scan the device for the Install Code
    • Enter Install Code Manually - You can manually enter the install code from the device
    After scanning or entering the install code, proceed to Step 6.

    TIP: It is recommended to add the device with Install Code for security.
  5. To pair the device without Install Code, tap Add Device without Install Code.
  6. Short press the top right push button 3 times.
    Make sure that the LED blinks orange.
  7. In the app, select Confirm that the LED is blinking (C) and tap Start configuration.

  8. After a few seconds, a solid green LED indicates that the device has been successfully paired to the Gateway.

  9. Once the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?