DUG_Exxact FLS_WSE-01

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
NOTE: Remember to insert the battery to turn on the device.
  1. Remove the rockers using a screwdriver to see the LED.
  2. On the Home page, tap +.
  3. Tap Auto scan > Confirm.
  4. Enable permissions to Access location and Wi-Fi for scanning device and tap Start scanning.
    NOTE: If you have multiple hubs, do Step 5 or proceed to Step 6.
  5. Tap Select hub and select the Wiser hub from the slide-up menu.
  6. Short press the top right push button 3 times and wait for a few seconds until the device search is completed.
    TIP: If you want to pair multiple devices, perform step 5 on each device and wait for a few seconds.
  7. Tap Next (A) and select Freelocate Switch.
  8. Tap Done once the device is paired successfully.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?