DUG_Exxact FLS_WSE-01

Technical Data

Battery

CR2032

Battery life

Up to 5 years (depending on frequency of use and quality of battery)

IP rating

IP20

Operating frequency

2405-2480 MHz

Max. radio-frequency power transmitted

<10 mW

Operating temperature

-5 °C to 45 °C

Relative humidity

5% to 95%

Communication protocol

Zigbee 3.0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?