DUG_Exxact FLS_WSE-01

2-gang with 2 Blind Control Switches

To pair the 2-gang Wireless switch with 2 blind control switches, you must change your Wireless switch to 2-gang operation. Refer to Switching from 1-gang to 2-gang operation.
NOTE: Do not remove the rocker of the blind control switches.
  1. Short press the right upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  2. Short press the first blind control switch 5 times in quick succession.
    The status LED blinks green.

    The shutter will move up and down for a few times. When successfully paired, the status LED on the Wireless switch and the blind control switch turns Off.
    IMPORTANT: Check if the pairing was successful before you continue with the left channel.
  3. Short press the left upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  4. Repeat step 2 on the second blind control switch.
    The shutter will move up and down a few times. When successfully paired, the status LED on the Wireless switch and the blind control switch turns Off.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?