DUG_Exxact FLS_WSE-01

Pairing 1-gang with 2 Blind Control Switches

NOTE: If you want to pair a 1-gang FLS with one blind control switch, follow the steps up to step 2. To continue with a second blind control switch, follow the next steps.
  1. Short press the upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.

  2. Short press the first blind control switch 5 times in quick succession.
    The status LED blinks green.

    The shutter will move up and down a few times. When successfully paired, the status LED on the Wireless switch and the blind control switch turns Off.
    IMPORTANT: Check if the pairing was successful before you continue with the same channel.
  3. Repeat step 1.
  4. Repeat step 2 on the second blind control switch.
    The shutter will move up and down a few times. When successfully paired, the status LED on the Wireless switch and the blind control switch turns Off.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?