DUG_Exxact FLS_WSE-01

Multiwire Micro Module Dimmer

Prerequisites: While connecting the dimmer to the mechanical push buttons, make sure that the terminal 1 of the dimmer is wired to the left mechanical push button, and terminal 2 of the dimmer is wired to the right mechanical push button.
  1. Short press the upper push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  2. WARNING
    HAZARD OF ELECTRIC SHOCK
    • Observe the regulations for working on live parts.
    • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    Follow either of the options to pair the Dimmer:
    • Short press the Setup/Reset button 5 times in quick succession on the Dimmer.
    • Short press the left push button (Wired to terminal 1) 5 times in quick succession.
    The status LED blinks green on the Dimmer.
    NOTE: If the Dimmer is located behind the mechanical push button, the status LED is not visible.

    The light connected to the Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Dimmer. The Dimmer can now be controlled by the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?