DUG_Exxact FLS_WSE-01

Adding a moment to the wireless switch

Using the Wiser app, you can add a moment to the Wireless Switch push buttons.
To add a moment to the Wireless Switch key(s):
  1. On the Home page, tap All devices > Connected Wireless Switch.
  2. On the control panel page, tap Top right key > Moment.
  3. Select a moment from the list of created moments (A).
  4. Short press the top right push button 3 times on the Wireless Switch to activate the device and tap Sure (B) on the app.

    The moment is now added to the Top right key (C).

    NOTE: If you add a lighting/shutter group to the bottom right key, then the app removes the moment from the top right key.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?