DUG_SysM/SysD_SSO_03

Checking the energy consumption

Using the Wiser app, you can monitor the energy consumption of the load connected to the device by accessing the consumption feature.
TIP: You can see the daily real-time energy consumption value of the load connected to the device on the control panel of the device.
To check the device energy consumption history:
  1. On the Home page, tap All devices > Connected Single Socket Outlet .
  2. On the device control panel page, tap Consumption.
  3. In the Consumption page, you can see the total energy consumption and it’s changes in Week (A), Month (B), and Year (C) view in the graph.
    You can tap each bar on the graph to see the total energy consumed on a particular day/month.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?