DUG_SysM/SysD_SSO_03

Example of an automation

This demonstration shows you how to create an automation to get notification on your app when the total energy consumption value of the Socket Outlet is 50 kWh.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Confirm.
    TIP: You can choose the cover image that represents your automation by tapping .
  3. Tap Add Condition > When device status changes > Connected Single Socket Outlet .
  4. Tap Daily Consumption, select the total energy consumption value (A) and tap Next.
    TIP: You can set the energy consumption value as 50 kWh.

  5. Tap Add task > Send notification and select Notifications (B).
  6. Tap Next.

  7. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
Push notification will appear on the screen when the automation is triggered. You can also tap on to access the notification history.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?