DUG_SysM/SysD_SSO_03

About the device

The Connected Single Socket Outlet 16A (hereinafter referred to as Socket Outlet) is a connected electrical outlet designed to manage and control electrical devices in a convenient and efficient manner. You can remotely control and monitor the energy consumption of the plugged-in load.

The Socket outlet is equipped with a temperature protection mechanism. When the Socket outlet is used with a high load over a long time, the mechanism can switch off the Socket outlet, ensuring overheat protection.

The Socket outlet is equipped with an overload protection mechanism. When the Socket outlet is used with a high load (18 A and high), the mechanism can switch off the Socket outlet, ensuring overload protection.

NOTE:
  • The device must not control safety-relevant applications

  • Do not mix different load types in the controlled socket

  • Do not use multi-sockets in the controlled socket

  • Do not use for EV charging

Operating elements

A: Push button with status LED

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?