DUG_SysM/SysD_SSO_03

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
To pair the device:
  1. On the Home page, tap +.
  2. Tap Auto scan and tap Confirm.
  3. If you have multiple gateways, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Short press the push button 3 times (< 0,5 s).
    NOTE:
    • The LED blinks amber.

    • Wait for a few seconds until the device search is complete.

    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds.
  6. Tap Next (A) and select Connected Single Socket Outlet 16A.

  7. Once the device is added successfully, tap Done.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?