DUG_SysM/SysD_SSO_03

Pairing the device with the Wiser Gateway

Using the Wiser app, pair your device with the Gateway/Hub to access and control the device. You can either add the device manually or do an auto-scan to pair it.
NOTE: The Socket Outlet shows a non-zero energy consumption value when the device is added to the app if the Socket Outlet was in ON state with a load connected before pairing it to the Gateway/Hub .
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?