DUG_SysM/SysD_SSO_03

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press the push button three times (< 0.5 s) and then long press the push button once (>10 s).
  2. After 10 s, LED starts blinking red then release the push button.
    The LED stops blinking upon successful reset of the device.
  3. The plug restarts and blinks green for a few seconds.
    NOTE: After reset, the LED stays amber.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?