Troubleshooting
Symptom |
Possible cause |
Solution |
---|---|---|
The Socket Outlet is not turning ON. |
The Socket Outlet is broken or it could be an alarm if the LED blinks red. |
Initially, turn off the socket outlet, disconnect it from the power supply and turn it on after some time. If it still not working, you can replace the socket outlet. For more information about the wiring refer to the installation instructions. |
When there is an alarm, the user cannot switch ON the output locally or remotely. LED blinks fast RED. |
Clear the Socket Outlet alarms. |
To clear the alarm, press and hold the push button for 4 seconds. After 4 seconds, the blinking will stop and the alarm will be cleared. You can use the Socket Outlet again. NOTE: Before clearing
the alarm, you must verify the reason for overcurrent fault and thermal
fault.
|