DUG_Micro Module Dimmer_WSE-02

Manual operation

When the puck is connected to a mechanical push button, the connected lighting devices can be controlled manually.

  • Short press the push-button rocker to turn on/off the light.

  • Press and hold the push-button rocker to adjust the dimming level of the light.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?