DUG_Micro Module Dimmer_WSE-02

Setting up a schedule

The devices can be fully controlled by schedule. Once the schedule is set, the devices operate at a given time.
To create a schedule:
  1. On the Home page, Tap All devices > Micromodule Dimmer.
  2. Tap Schedule > Add Schedule to add a schedule.
  3. In Add Schedule menu, set the time (A).
    NOTE: The Schedule works according to the time zone where the device is located.
  4. Tap Repeat (B) to select the days you want to set the schedule.
  5. Tap Note (C), enter the note and tap Confirm.
  6. Tap the toggle switch (D) to turn on the Notification for the schedule. The app will send a notification that the scheduled task is executed at the time of schedule.
  7. Adjust the Brightness settings (E) through sliding bar.

  8. Tap Save
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?