DUG_Micro Module Dimmer_WSE-02

Resetting the device

You can reset the device to factory default manually.
To reset the device:
  1. Short press the Setup/Reset button three times (< 0.5 s) and then long press the Setup/Reset button once (>10 s).
    or
    Short press the push button 3 times and then long press the push button once for 10 s.
  2. After 10 s, LED starts blinking red then release the operation button.
    NOTE: All configuration data, user data, and network data are deleted. After which
    • No connectivity to other devices or rooms.

    • No timer settings.

    • Memory function is active.

    • Automatic load detection is active, RC mode is set.

    • No limitation to dimming range.

    The LED stops blinking upon successful reset of the device.
  3. The Puck restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns orange indicating that the device is ready for pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?