DUG_Micro Module Dimmer_WSE-02

Setting the minimum and maximum brightness level

If the dimmer is connected to an LED, the minimum and maximum brightness should be set to avoid flickering and switching off the LED.
To set the minimum and maximum brightness level:
  1. On the Home page, Tap All devices > Micromodule Dimmer.
  2. Tap .
  3. Tap Dimming Range for slide-up menu.
  4. Drag the sliding bar to increase or decrease the Minimum Brightness and Maximum Brightness (A).

  5. Tap Close(B).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.