DUG_Micro Module Dimmer_WSE-02

For your safety

DANGER
Hazard of electric shock, explosion, or arc flash
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks.
  • Connecting several electrical devices.
  • Laying electric cables.
  • Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock
  • Make sure that the terminal connection area does not come in contact with the metallic parts of any device installed in the same location.
  • Do not short the outputs to neutral.
Failure to follow these instructions will result in death or serious injury.
CAUTION
equipment damage
  • Always operate the product in compliance with the specified technical data.
  • Never connect any mixed inductive/capacitive loads.
  • Connect only dimmable loads.
  • Do not connect the dimmer output to the socket outlet.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?