DUG_Micro Module Dimmer_WSE-02

Testing the device

Before using the Puck, manually test the Puck and make sure that it works when connected to the lighting devices.
WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  • Short press the test button once, the connected lighting device turns On/Off.

  • Press and hold the test button to adjust the dimming level of the connected lighting device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?