DUG_Micro Module Dimmer_WSE-02

Creating a moment

A Moment allows you to group multiple actions that are usually done together. Using the Wiser app, you can create moments based on your needs.
To create a moment:
  1. On the Home page, tap .
  2. Go to Moment > + to create a moment.
  3. Tap Edit name (A), enter the name of the moment and tap Save.
    TIP: You can choose the cover image that represents your moment by tapping .

  4. In the Action section, tap Add task (B) to open the slide-up menu.
  5. In the Add task menu, you can do either or all of the following actions (C):
    • Run the device - Select the devices that you want in a moment.
    • Select Automation - Select the automation that you want to enable or disable.
    • Delay - Set the delay time.
    NOTE: You can add one or more actions using .

  6. Tap Run the device > Micromodule Dimmer to select either or all the functions to add in the moment:
    • Dimmer (D) : To set the device On/Off.
    • Brightness (E) :To set the percentage of brightness required.

  7. Tap Next and once the actions is set, tap Save.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.