DUG_EVlink_WH-06

Charging mode

Using the Wiser Home app, you can manage the mode of charging.

  1. On the Control tab, tap All devices > EV Charger.

  2. On the device control panel page, tap Charging Mode.

  3. On the EV Charging Mode menu, select any one of the following options:

    1. Manual: charging will start as soon as the cable is plugged in to Electric vehicles (EV).

    2. Wiser Home AI: your electric vehicle will automatically start charging at the next cost effective time period based on the tariff to reduce your total cost of charging.

      IMPORTANT: This feature is applicable only when there are suitable tariffs created. Refer to Wiser Home AI and Tariff plan configuration.
    3. Customized Schedule: create your own schedule to charge your electric vehicle.
      Refer to Creating a schedule.

    NOTE: For more information on Wiser Home AI and Setting Tariff refer to the respective System User Guide.

NOTE: You can change the charging mode at any time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?