DUG_EVlink_WH-06

Using the device

The Control Panel allows you to start and stop charging and monitor the power consumption.

On the Control page, tap EV Charger to access the control panel.

On the control panel page, you can see the following:

  • Total cost of charging session (A).

  • Total time of charging in the session (B).

  • Total energy consumption in the session (C).

  • Control button (Start charging/Stop charging, Pause/Resume) (D).

  • Charging Mode (E).

  • Device settings (F) - You can rename the device or remove the device from the Wiser system. Refer to Renaming the device and Removing the device.

  • History (G).

Similarly you can control and check the current status of EV from Control page.

  • Control button (H).

  • Current state of the device (I).

TIP: You can also start and stop charging when you add the device to your Favorite list. For more details about Favorites, refer to the respective System User Guide.
NOTE:
  • If you only have an EV Charger in the Wiser System, the Control page will not be visible. All functions will be accessible through the Home page.

  • Electric vehicles (EV) can't be charged immediately after they have stopped. Reconnect the plug to start charging. Refer Connecting/disconnecting the charger.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?