DUG_Mureva EVlink_Socket_WH-04

Using the device

The EV Socket Control Panel allows you to start and stop charging and monitor the power consumption.
IMPORTANT: Must use Mode 2 cable (max 16 A - 3.7 kW) cable from the EV Socket to connect your car.

On the Control tab, tap All > EV Charger to access the control panel.

On the control panel page, you can see the following:

Similarly you can control and check the current status of EV Socket from Control tab.

  • Control button (H).

  • Current state of the device (I).

TIP: You can also start and stop charging when you add it to your Favourites. To know more about Favouritse, refer to the Manage Favourites topic in the respective System User Guide.
NOTE: If you only have an EV Charger in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?