DUG_Odace - Thermostat 2 A_WH-07

About the device

The Odace - Connected Thermostat 2 A (hereinafter referred to as thermostat) is mainly used for water-based heating and cooling applications, such as water-based underfloor heating and radiator heating.

Thermostat features:

  • Measure & control the room temperature

  • Dot-matrix displays (current room and set temperature)

  • Device lock

  • Valve Protection

  • Heat/cool changeover

  • Volt-free or live control, normally open or normally closed.

  • Smart schedule through a Wiser Home app

Operating elements

  1. Dot-matrix display

    • Wireless connectivity LED ()

    • Heat and cool demand LED ()

    TIP: All LED indications are explained in the LED behavior chapter.
  2. Touch button: + and

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?