DUG_Odace - Thermostat 2 A_WH-07

Editing a Moment

Using the Wiser Home app, you can edit the existing Moment, and you can change the thermostat settings.
  1. On the Automation page, tap Moments tab.

  2. Select the moment that you want to modify.

  3. On the Moment editor page, you can do the following:

    • Rename a moment

    • Delete a moment

    • Add actions

    • Change the device settings

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?