Device presetting
You can choose one of three preset configurations:
| Preset | Configuration | Cycle Time* (min) | Valve Protection |
| P1 | Heat Pump/Oil Boiler | 20 | Off |
| P2 | Hydronic Radiator/Gas Boiler | 10 | Off |
| P3 | Hydronic Underfloor | 10 | On |
*Cycle time:: This setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor. A short cycle time is more appropriate for faster heating surfaces, such as an electric panel heater.
Initial preset configuration (by default)
When the thermostat is first powered
on or immediately after a factory reset, by default “P1” flashes on the matrix LED’s to indicate Preset (P1) is selected to provide initial configuration.
Modifying the preset value
When + button is pressed, it increases the
preset value by 1 and pressing - button, it decreases the preset
value by 1.
For example, when
+ button is pressed, preset P1 becomes P2, continue to press the +
button, and the preset changes to P3.
Similarly, when – button is pressed, preset P3 changes to P2, continue to press the – button, preset changes to P1.
Confirming the preset
Select the preset that meets your needs using the +/- buttons, and then hold the +/- simultaneously for
> 1 s to confirm the selection.
For example, P1 is confirmed.