Dimmer
|
A |
Device Name: Tap to change the name of the device. |
|
B |
Location: Tap to assign the Dimmer to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location. |
|
C |
RL-LED Mode: You can enable RL-LED Mode if the 1-gang dimmer is connected to an LED lamp. It is recommended using this mode when you experience flickering of the bulb. Verify the lamp manufacturer’s specifications and the reduced power of the dimmer. |
|
D |
LED Indicator Behaviour: Tap to set the LED indicator behaviour of the dimmer as per your preference. Refer to Setting up the LED Indicator Behaviour for detailed information on each options. |
|
E |
Power On Behaviour: Tap to set the default brightness level of the dimmer when it is turned on. Refer to Setting up the Power On Behaviour for detailed information on each options. |
|
F |
Minimum Brightness and Maximum
Brightness: This setting lets you set limits on the maximum
and minimum brightness of the connected load. This is done to avoid
flickering and switching off the LED. IMPORTANT: If the light does not begin to brighten up from 0%, adjust the minimum
level setpoint to the point where the light actually starts to brighten.
Similarly, for maximum brightness, set the maximum level based on
the behaviour of the connected light. For example, if brightness does
not increase between 80% and 100%, then set the maximum level to 80%.
NOTE: The minimum brightness must be lower than the maximum brightness.
|
|
G |
Identify: Tap to identify the device. NOTE:
|
|
H |
Delete: Tap to remove the device from the system. |
|
J |
Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device. |