DUG_Push-button Module, 1-gang/2-gang_WH-08

LED indications

Pairing the device

User Action

LED Indication

Status

Press the push button 3 times.

LED blinks amber, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off.

Resetting the device

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts, and the LED glows solid orange.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?