DUG_Push-button Module, 1-gang/2-gang_WH-08

Shutter

Using the Wiser Home app, you can rename the 1-gang shutter, edit or assign a new location, identify, and delete the 1-gang shutter from the system.
NOTE: There is no 2-gang switch available for shutter operation.
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > 1-Gang to locate to Device Details screen.

    A

    Device Name: Tap to change the name of the device.

    B

    Location: Tap to assign the shutter to any room (such as living room, bedroom, kitchen etc). Refer to Setting the device location for more details on how to set the location.

    C

    Device Type: Tap to change the device type according to your need. Refer to Selecting device type for detailed information on each options.

    D

    Open duration and Close duration: Tap to set the default run time to open/close the shutter. Refer to Setting the configure duration for detailed information.

    E

    Identify: Tap to identify the device.

    NOTE:
    • The status LED blinks red and the shutter opens/closes gradually, upon successful identification of the 1-gang shutter or shutter slat.

    • The 1-gang shutter LED will continue to flash until you tap OK.

    F

    Delete: Tap to remove the device from the system.

    G

    Zigbee Signal Strength Indicator: Zigbee Signal Strength indicator which displays the current signal strength of the device.

    • Good Signal (between 0 & -54dBm)

    • Normal Signal (between -54 & -79dBm)

    • Poor Signal (<-79dBm)

    • No Signal (device is offline)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.